ATI Industrial Automation   ATICombinedDAQFT .NET Class Library  

Visit our website.

SetForceUnits( forceUnits As String) As Integer

Set the units of the force outputs.

Arguments

forceUnits

In: The force units to output in. Acceptable values are "lb","klb","N","kN","g", or "kg".

Returns

0: successful completion
1: calibration not initialized (call LoadCalibrationFile before calling this function )
2: invalid force units specified

See Also

LoadCalibrationFile